cancel
Showing results for 
Search instead for 
Did you mean: 

Temperature vs efficiency curve and MTBF data for SPV1040

shalinich67
Associate II
We are currently evaluating the following STMicroelectronics IC for our application:
SPV1040TTR
As part of our reliability and performance assessment, we kindly request your support in providing:
  1. Temperature vs. efficiency curves across the specified operating temperature range
  2. MTBF (Mean Time Between Failures) data or estimated MTBF hours for the above-mentioned ICs
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

You have already created a ticket with the internal ticket number 00254037 today, and I would ask you to wait for a response from that team. The community will not really be able to help you with your question, as it is a global forum for mutual assistance between users.

Thank you for your understanding and patience.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
Peter BENSCH
ST Employee

You have already created a ticket with the internal ticket number 00254037 today, and I would ask you to wait for a response from that team. The community will not really be able to help you with your question, as it is a global forum for mutual assistance between users.

Thank you for your understanding and patience.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
shalinich67
Associate II

Can I get the related information please

As I can see now, the OLS team has referred you to the community, which is definitely not correct. However, I can already say that an NDA (Non Disclosure Agreement) is necessary to get MTBF data, which definitely has to be handled via the OLS.

However, regarding your first question, I cannot give you any hope of obtaining efficiency curves, especially over temperature, because this depends on a great many external parameters. Among other things, the number of cells to be charged plays a very important role. The device was launched on the market back in 2010, so the probability of such a data sheet supplement is virtually zero.

Regards
/Peter

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Can you atleast provide with the junction to case thermal resistance (Rthjc) for the IC.

Thanks.

Actually, this does not directly relate to the original topic and would require a separate thread. Nevertheless, I will briefly address your new question:

Because for a small plastic package like TSSOP‑8 without exposed pad, the heat path to the ambient is dominated by junction > leadframe > pins > PCB > ambient, not by junction > case (top). In that situation Rthjc​​ (junction-case, usually to the top surface) is poorly defined, not very useful for real applications and easily misleading.

ST therefore specifies only Rthj-ambient, measured on a standard PCB, because this reflects the realistic use case: the part soldered on a board where the PCB copper does most of the cooling. The value for Rthja is specified in the data sheet and is 135K/W.

Hope that answers your additional question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.