2021-06-21 12:19 AM
Hello,
ist there an SPI example available to control the L9026 for switching 8 solenoids?
Or even an example how to define the HEX command i have to send via SPI especial only to switch all 8 channels on and off.
2021-08-04 09:34 AM
hello,
sorry but examples of configuration via SPI are not available.
In case, if you want to switch on channels via SPI just write the relative bits in the register to "1": PWM_SPI, as reported in chapter 12.6 “SPI registers�?.
regards.
Elena