cancel
Showing results for 
Search instead for 
Did you mean: 

sensored BLDC motor for X-NUCLEO-IHM16M1

JD.1720
Associate II

I recently purchased the NUCLEO-F303RE and X-NUCLEO-IHM16M1 development kit.

With a 2804 Gimbal motor.

So far all the tests have gone well for me.

But my intention is to control a sensored BLDC motor.

Do you know of any sensored BLDC motor that works well with this development kit?

Thanks!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
JD.1720
Associate II

I have tried the following sensored BLDC motor R30BLB4L1 and it worked correctly for me.

View solution in original post

3 REPLIES 3
Cristiana SCARAMEL
ST Employee

Hello @JD.1720​ and welcome to the ST Community.

I cannot suggest a brand but only to choose a three-phase brushless motor with compatible voltage and current for the STSPIN830 driver.

If you want to use the kit power supply the voltage ratings is reduced to 12 V (nominal value).

Otherwise you can use an external power supply with output voltage between 7 and 45 V (CN1 or Ja connectors).

Concerning the X-NUCLEO-IHM16M1 hardware settings you can refer to the user manual UM2415.

Let’s see if other Community Members can suggest you a specific motor part number that they used.

If you feel a post has answered your question, please click "Accept as Solution"
JD.1720
Associate II

Thanks for help

JD.1720
Associate II

I have tried the following sensored BLDC motor R30BLB4L1 and it worked correctly for me.