Reverse Power flow for LD39050 regulator, what will it affect
Hello everyone,
I have a question, and i hope someone can help me,
I am currently building a circuit which contains 2 source of power;
1- main source (3V CR2 battery)
2- auxiliary source (5V USB in case of emergency)
taking into consideration that all the circuit is 3v tolerant, i needed to add a regulator when using emergency power (LD39050PU33R),
the question is if circuit is operation from battery and the regulator is having reverse power flow (3v input from battery and the vout pin) however the regulator is disabled,
How that will affect the circuit and how can take the necessary design actions if needed?
Thank you