cancel
Showing results for 
Search instead for 
Did you mean: 

Reverse Polarity with ST1S14

EN11
Visitor

EN11_0-1738929544771.png

Hello I have created reverse polarity but it can not work stable especially in the first work , this time I change the voltage a little bit it works :) ı cant understand.

What should ı do?

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome @EN11, to the community!

  • What output current do you want to draw at -15V_O?
  • What is the saturation current of L2?
  • Can you please show the layout so that this can be checked?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I am using the just supply for opamps , and also ı guess understand problem is a lot capacitors ı put the resistor in the output problem seems to be solved.

but ı continue to try .

Best Regards.