2025-05-10 8:33 PM - last edited on 2025-12-29 12:18 PM by ELABI.1
Hello ST Community,
I am currently working on a project involving a fuel dispenser control panel and have been prototyping using the STM32F407VGT6 Discovery board. During the development phase, I connected the following peripherals:
OLED display via I2C
External EEPROM (24CXXX series)
4x5 matrix keypad
RS485 transceiver via USART2 (TTL to RS485)
RS422 transceiver via USART3 with DE/RE control on pin PD13
As the prototype phase is nearly complete, I am now preparing to design a custom PCB based on the STM32F407VGT6 microcontroller.
I kindly ask for a recommended reference schematic or design guidelines that cover the essential external circuitry for the STM32F407VGT6, specifically:
Power supply filtering and regulation (including recommended capacitors, analog/digital separation, VCAP, etc.)
Clock configuration (main crystal oscillator, RTC crystal, load capacitors)
NRST and BOOT0 pin handling
Any other critical hardware considerations to ensure reliable operation of the MCU in standalone configuration.
I will be handling the external peripherals separately, so only the core MCU circuitry is needed.
If ST provides a minimal schematic or application note that is suitable for this case, I would appreciate it if you could share the link.
Thank you in advance for your support and best practices!
Best regards,
Azizbek
2025-05-10 8:53 PM
Here is the STM32F4 hardware design guide which covers all of these things.
Getting started with STM32F4xxxx MCU hardware development - Application note
There are also a number of boards from ST from which you can use schematics for reference. Here is one of them:
https://www.st.com/en/evaluation-tools/stm32f4discovery.html#cad-resources