2021-09-05 10:41 PM
I'm mounting SPV1050 on PCB. In my application, I'm using a PV cell as input to the IC and takes the output from Vbatt to charge a battery. I am not using LDO or anything extra.. no use of store too. Is it right if I make Pin 5,6,7,8,11,12,17 open circuit?
Solved! Go to Solution.
2021-09-05 11:35 PM
Pins 5 and 6 are inputs (LDO1_EN, LDO2_EN) and should be connected to GND when the LDOs are not used.
You can leave the remaining pins floating.
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
Good luck!
/Peter
2021-09-05 11:35 PM
Pins 5 and 6 are inputs (LDO1_EN, LDO2_EN) and should be connected to GND when the LDOs are not used.
You can leave the remaining pins floating.
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
Good luck!
/Peter
2021-09-05 11:50 PM
Pin 7 and 8 should be floating right? Are you sure?
2021-09-06 12:35 AM
Yes, pin 7 (BATT_CHG) and pin 8 (BATT_CONN) are outputs and indicators that can but do not have to be used.
Regards
/Peter