2005-07-16 09:32 PM
question about the output voltage of L6208
2011-05-17 01:18 AM
The supply voltage for L6208 is 13V
CP input : 2k HZ step motor :42BYG016(a bipolar stepper---12V/0.3A) but the output voltage in pin outA1 is only 5V(step motor work normally without load ) why is so low ? as I set the supply voltage on 24V the output is about 11V and the circut is the one in the L6208's application note the output voltage what I expected in this circut is 10-12V when the supply voltage is 12-15V another question is :how to increase the output voltage for the step motor and what parameter in L6208 decide the output voltage ? [ This message was edited by: kelvin9527 on 17-07-2005 10:17 ]