cancel
Showing results for 
Search instead for 
Did you mean: 

PMIC for 24V with ASIL D SPI and watchdog

SU1
Associate

We need PMIC for Automotive application with 24V with SPI and watchdog with ASIL D

2 REPLIES 2
SU1
Associate

Kindly reply to the above PMIC requirement

Peter BENSCH
ST Employee

Welcome @SU1, to the community!

With your given parameters you can have a look at the following PMICs:

They can be operated with a VBAT of up to 32V. But you probably need a higher input voltage range because of the expected load dump tests, don't you?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.