cancel
Showing results for 
Search instead for 
Did you mean: 

PM6670AS current consumption

eamonn2
Associate II
Posted on October 02, 2013 at 19:11

Hi,

I am thinking of using a PM6670AS to power DDR3 memory on a new Virtex-7 board. Can someone tell me what will be the maximum current consumed on the VCC and AVCC +5V pins? This must be with the S3 and S5 pins connected to AVCC, a nominal load (<1mA) on Vttref, the Mode pin tied to AVcc and the DDRSEL pin tied to ground (1.5v operation).

Thanks,

Eamonn Walsh

#pm6670as #pm6670
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0