cancel
Showing results for 
Search instead for 
Did you mean: 

output current of ISO808

ny851
Associate II

hello 

we are going to use ISO808 IC in our project according to the datasheet of ISO808 Short circuit protection on output channels ( ILIM(MIN) )is 0.7A but for Channel Output Current (continuous) it is mentioned as internally limited. could you please provide a data for continuous maximum output current per channel at 25 C ambient temperature or Is there any formula to calculate per channel continuous output current at particular ambient temperature. 

Best regards,
Nisha Yadav

1 REPLY 1
ny851
Associate II

Hello Team,

Any update on this?