2023-08-31 5:29 AM - last edited on 2023-08-31 10:57 AM by Peter BENSCH
hello
we are going to use ISO808 IC in our project according to the datasheet of ISO808 Short circuit protection on output channels ( ILIM(MIN) )is 0.7A but for Channel Output Current (continuous) it is mentioned as internally limited. could you please provide a data for continuous maximum output current per channel at 25 C ambient temperature or Is there any formula to calculate per channel continuous output current at particular ambient temperature.
Best regards,
Nisha Yadav
2023-09-06 5:41 AM
Hello Team,
Any update on this?