2009-01-15 11:37 PM
Need suggestion for Stepper/servo motor controller with encoder !!!!!
2011-05-17 1:15 AM
Hi friends,
We are planning to shift from ''SILAB 8051 + Keil C51'' to ARM (cortex-M3), for my new project 5-Axis CNC controller . In that we have to generate pulses up to 2MHz & quadrature encoder for position sensing. We have two options, 1. Luminary micro -> They have inbuilt dedicated motion control & quadrature encoder interface. 2. STM32 -> In STM32, which processor is suitable, Will I need some peripherals to implement above requirement ???????? Thanks in advance, Kishor. [ This message was edited by: kishhor on 17-01-2009 12:25 ]