cancel
Showing results for 
Search instead for 
Did you mean: 

L6470 full-step mode and absolute position

johan
Associate
Posted on May 06, 2013 at 18:19

Hi,

Does the L6470 maintain the validity of the ABS_POS value during automatic full-step operation? I want to position my motor with 1/16 microsteps but still be able to run 1500 rpm.

BR, Johan

#l6470
1 REPLY 1
Enrico Poli
ST Employee
Posted on May 08, 2013 at 15:37

Sure. Even if the system switches to the full-step mode, the ABS_POS register indicates the position with the programmed microstepping resolution.

Enrico