2011-08-18 12:35 PM
L6470: connect Vreg and Vdd for 5V supply?
#l6470 #l64702011-08-18 12:42 PM
2011-08-29 12:34 AM
For 5V supply voltage:
VREG connected to 3.3V or internally supplied (in this case plase a capacitor on Vreg pin)VDD connected to 5V
2012-01-05 7:42 AM
If using 5V only for Vdd
What value cap(s) are recommended for a open (using Internal 3.3V reg) Vreg pin Thanks Joe2012-01-10 1:43 AM
Dear Joe,
The VREG pin needs at least a 22uF capacitor to be stable. The recommended value is 47uF.If you want to use a electrolytic cap, I also suggest you to add a small ceramic cap (100nF) to filter the current spikes coming from the logic.The VDD need a 10uF capacitor.Kind RegardsEnrico