2022-02-24 8:18 PM
Solved! Go to Solution.
2022-02-25 1:18 AM
There are UL certificates only for safety-relevant features. Non-insulated transistors such as the STW4N150 have electrically accessible metal parts, which is why no UL certification is granted for them.
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2022-02-25 1:18 AM
There are UL certificates only for safety-relevant features. Non-insulated transistors such as the STW4N150 have electrically accessible metal parts, which is why no UL certification is granted for them.
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2022-02-25 1:39 AM
Got it, Thanks.