cancel
Showing results for 
Search instead for 
Did you mean: 

I am usind LD1085 voltage regulator connected to a 500mA of load. When the capacitor connected is 100uF at both i/p and o/p it is becoming too hot with 30-50 sec. Same is the condition with 10uFcapacitor at i/p and o/p and also with 22uF at i/p and 47uFa

IRBAZ RASHID
Associate
Posted on April 11, 2017 at 07:21

I am using LD1085  voltage regulator connected to a 500mA of load. When the capacitor connected is 100uF at both i/p and o/p it is becoming too hot within  30-50 sec. Same is the condition with 10uFcapacitor at i/p and o/p and also with 22uF at i/p and 47uFa

0 REPLIES 0