cancel
Showing results for 
Search instead for 
Did you mean: 

I am planning to use the STEVAL-ILL078V1 board for driving infra-red LEDs. Components will be changed to match values in the attached eDesignSuite printout. Would it be possible to replace "Rlim" with a digital potentiometer to make changes on the fly?

CRAMF.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Peter BENSCH
ST Employee

Welcome, @CRAMF.1​, to the community!

Yes, you can also use a polycrystalline digital potentiometer as a RILIM instead of a fixed resistor. The important thing is that it is a real ohmic resistor and not a semiconductor junction whose behaviour may not be suitable.

However, please keep an eye on the non-linear characteristic of ISKIP current vs. RILIM, so that you do not overload the IRLED.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Peter,

Thank you for confirming. I was waiting for your reply before looking into the details of the resistive properties provided by digital potentiometers. If the latter do not come with ohmic output resistances then I might look at using a 1x8 multiplexer connected to a various resistances. I am currently busy with another project and I may get back to you if I have additional questions regarding the ISKIP parameter you have mentioned below. Thank you for the heads-up!

Chundra Ramful, P.Eng.

[ personal information removed by moderator ]