2023-02-08 4:12 AM
How to implement LTC4015 with Stm32L072 MCU, I want to charge the battery through LTC4015 using I2C. Can you please suggest me how to use this in stm32 microcontroller.
Solved! Go to Solution.
2023-02-08 7:32 AM
Hello @jm.2 ,
If we look at the datasheet of the LTC4015 :
Finally, open STM32CubeMx and start the configuration. :D
I recommend you this WIKI : Getting started with I2C - stm32mcu ,It will help you for the configuration.
Hope my answer helped you!
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-08 7:32 AM
Hello @jm.2 ,
If we look at the datasheet of the LTC4015 :
Finally, open STM32CubeMx and start the configuration. :D
I recommend you this WIKI : Getting started with I2C - stm32mcu ,It will help you for the configuration.
Hope my answer helped you!
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-12 11:29 PM
Thank you. But no useful =)
2023-02-24 1:47 AM
Hi sir,
Can you please tell me how to send the LTC4015 commands in stm32. If you have any sample code means send me. Please help me on this.
Thanks in advance.
2023-02-24 1:56 AM
Hello ,
Battery charge voltage is pin selectable and I 2C adjustable. Input current limit and charge current can be accurately programmed with sense resistors and can be individually adjusted via the I2C serial port
So you can try to manage your application via I2C commands :
/* Write an amount of data in blocking mode to a specific memory address*/
HAL_I2C_Mem_Write(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint16_t MemAddress, uint16_t MemAddSize, uint8_t *pData, uint16_t Size, uint32_t Timeout);
/*Read an amount of data in blocking mode from a specific memory address*/
HAL_I2C_Mem_Read(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint16_t MemAddress,uint16_t MemAddSize, uint8_t *pData, uint16_t Size, uint32_t Timeout);
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-24 2:21 AM
How to implement this, can you please tell me.
2023-02-24 2:49 AM
First of all, please
Open STM32CubeMx and start the configuration.
Generate code (choose your IDE)
HAL_I2C_Mem_Read(&hi2c1, DevAddress, 0x15,1, (uint8_t*)(®ister_value), 1, 1000);
Hope my answer helped you!
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-24 3:33 AM
Thanks for quick response.
Yeah I understood, how to implement, but I have one more doubts please help me don't take mistake, my doubt is what registers and all I have to use to charge the battery, please help me.
2023-03-01 8:18 PM
Hi,
I am waiting for your reply.