cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I'm looking for the solution that can take 5V solar panel input and charge 4.2V lithium battery.

ezuk
Associate

Hi,

I'm looking for the solution that can take 5V solar panel input and charge 4.2V lithium battery. I also need to be able to provide the power to the rest of the system even when the battery is not connected. I was looking at SPV1050 IC but I'm not sure if I can use it with a load. Any suggestions?

Thanks!

Emilija

0 REPLIES 0