2021-07-19 10:49 PM
I am using 12V motor, all the phase I measured 12V, its look like it stuck at brake.
what can be the problem?
I am using motor 1028m012b - FAULHABER
Solved! Go to Solution.
2021-08-08 1:07 AM
Hi,
I am using PWM with FWD/REV input.
sometimes the motor stucked and not moving.
I am rotating the motor with my hand and after power on the driver, the motor is moving.
I don know why sometimes the motor not moving.
2021-09-01 9:16 AM
Hi @IGAL TALOR,
so in summary, the solution to your original question was to replace the damaged motor (Hall effect signal missing), right?
If I understand well, we can consider closed this topic.
Please open a new topic for a new question.
2021-09-01 8:50 PM
No.
I found another mistake at the evaluation board and the schematic.
the correct connection:
OUT3 J5-3 to motor pin 3
OUT2 J5-2 to motor pin 2
OUT1 J5-1 to motor pin 1
I checked with fluke between the IC to the J5 connector, the schematic is not correct.
now the motor is moving well with PWM with FWD/REV signal.
2021-09-01 11:56 PM
Hi @IGAL TALOR ,
I had already reported in a previous posts (July 20) how to connect the motor properly to the J5 connector.
There is no a misalignment between board an schematic, the silkscreen near the connector indicates the IC OUT number, not the J5 poles number.
Anyway, now the motor is running, fine!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.