2021-07-19 10:49 PM
I am using 12V motor, all the phase I measured 12V, its look like it stuck at brake.
what can be the problem?
I am using motor 1028m012b - FAULHABER
Solved! Go to Solution.
2021-08-08 1:07 AM
Hi,
I am using PWM with FWD/REV input.
sometimes the motor stucked and not moving.
I am rotating the motor with my hand and after power on the driver, the motor is moving.
I don know why sometimes the motor not moving.
2021-09-01 9:16 AM
Hi @IGAL TALOR,
so in summary, the solution to your original question was to replace the damaged motor (Hall effect signal missing), right?
If I understand well, we can consider closed this topic.
Please open a new topic for a new question.
2021-09-01 8:50 PM
No.
I found another mistake at the evaluation board and the schematic.
the correct connection:
OUT3 J5-3 to motor pin 3
OUT2 J5-2 to motor pin 2
OUT1 J5-1 to motor pin 1
I checked with fluke between the IC to the J5 connector, the schematic is not correct.
now the motor is moving well with PWM with FWD/REV signal.
2021-09-01 11:56 PM
Hi @IGAL TALOR ,
I had already reported in a previous posts (July 20) how to connect the motor properly to the J5 connector.
There is no a misalignment between board an schematic, the silkscreen near the connector indicates the IC OUT number, not the J5 poles number.
Anyway, now the motor is running, fine!