cancel
Showing results for 
Search instead for 
Did you mean: 

hi, I am using L298 . I am driving 2 phase stepper motor with 4A. it's the parallel mode. I have parallel stages 1-2 and stages 3-4. unlike fig. 7 in the datasheet. and The stepper motor works well. Does this method damage the IC in the long run?

A.Reza
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @A.Reza​, to the community!

The datasheet recommends paralleling channel 1 with 4 and channel 2 with 3: the thermal load on the output stages is thus better distributed on the chip.

It works with your design, but the resulting temperatures will be more concentrated (chip hot spots). It is therefore advisable to follow the instructions in the datasheet.

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome, @A.Reza​, to the community!

The datasheet recommends paralleling channel 1 with 4 and channel 2 with 3: the thermal load on the output stages is thus better distributed on the chip.

It works with your design, but the resulting temperatures will be more concentrated (chip hot spots). It is therefore advisable to follow the instructions in the datasheet.

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
A.Reza
Associate

Hi Peter, It was a very informative point.

Thank you for your attention and speed of response.

Good luck