cancel
Showing results for 
Search instead for 
Did you mean: 

Help to identify PS

anagy9
Associate II

Hi all,

Is anybody known something about this power supply? What I know is:

  • There is an ST logo on the board.
  • Input: ~240VAC
  • Output: 12VDC
  • using 1NK60Z and TL431 in TO92 package

There are four component blown out. One of the blown out 3 pin component marking starts by ,F'. The other 3 resistors(?) are unidentifiable. If it is a custom supply, is there any what similar with this what can help me to identify broken parts?. I think the age of it is about 8-10 years.

0690X000008j49cQAA.jpg0690X000008j49XQAQ.jpg0690X000008j49hQAA.jpg

Thank you!

Attila

1 REPLY 1
BRYAN SPEED
Senior

The clue as to who built and possibly designed the overall PS Unit is facing you in text in last picture :) you might ask them :)