2025-06-03 10:57 PM - last edited on 2025-06-04 12:04 AM by Andrew Neil
大家好,
我目前正在研究基于 STWBC50-HP 芯片的 2W 无线功率发射器。我的目标是在不使用 Qi 协议的情况下验证硬件功能,用于学习和测试目的。
我已经完成了发射器硬件设计,现在正在努力寻找一种无需 Qi 通信即可输出固定功率的固件,例如演示或示例项目,例如:
STWBC2-FW-固定功率输出、或任何允许恒定功率输出(例如,19V 2.6A)而无需协议协商的类似固件。
不幸的是,我在 ST 网站资源或 STM32Cube 软件包中找不到确切的固件。
任何人都可以分享下载链接或提供在哪里找到此固件的建议吗?
此外,如果有任何官方指南或步骤将 STWBC2-HP 配置为固定功率模式,那将非常有帮助。
提前致谢!
2025-06-04 12:10 AM - last edited on 2025-06-04 12:23 AM by Andrew Neil
Duplicate - merged.
Thanks for the translation.
Hello everyone,
I'm currently working on a 50W wireless power transmitter based on the STWBC2-HP chip. My goal is to verify hardware functionality without using the Qi protocol, for learning and testing purposes.
I have completed the transmitter hardware design and am now trying to find a firmware that can output fixed power without needing Qi communication, such as a demo or example project like:
STWBC2-FW-FixedPowerOutputor any similar firmware that allows constant power output (e.g., 19V @ 2.6A) without protocol negotiation.
Unfortunately, I couldn’t find the exact firmware in the ST website resources or STM32Cube packages.
Can anyone share a download link or provide suggestions where to find this firmware?
Also, if there are any official guidelines or steps for configuring STWBC2-HP for fixed power mode, that would be very helpful.
Thanks in advance!