Skip to main content
BPara.1
Associate
April 26, 2022
Solved

Hello. My question would be: can I control the speed on the steval ptool 1v1 board with a pwm signal or just an analog voltage? Or it is possible to give a pwm signal to the analog input? Thanks in advance for the answer. Bela

  • April 26, 2022
  • 1 reply
  • 611 views

..

This topic has been closed for replies.
Best answer by Cristiana SCARAMEL

Hello @BPara.1​,

you have different options to generates the VSPEED voltage signal (PA3):

  • connect an external trimmer to J9 connector (replacing R18 with 0 ohm)
  • apply an analog voltage value at J9 connector (between 2 and 3 pins)
  • apply a PWM signal at J9 connector (setting a proper value for the R19-C18 network)

I hope this post can help you; if so, consider to mark it as best answer by clicking the label "Select as Best".

1 reply

Cristiana SCARAMEL
ST Employee
April 27, 2022

Hello @BPara.1​,

you have different options to generates the VSPEED voltage signal (PA3):

  • connect an external trimmer to J9 connector (replacing R18 with 0 ohm)
  • apply an analog voltage value at J9 connector (between 2 and 3 pins)
  • apply a PWM signal at J9 connector (setting a proper value for the R19-C18 network)

I hope this post can help you; if so, consider to mark it as best answer by clicking the label "Select as Best".

"If you feel a post has answered your question, please click ""Accept as Solution"""