2020-06-08 03:10 AM
2020-06-08 08:52 AM
Hello, from your data I can suggest the EVSPIN32F0251S1 board.
It is a 3-phase complete inverter based on the STSPIN32F0251 controller, which embeds a 3‑phase 250 V gate driver and a Cortex®‑M0 STM32 MCU.
The power stage features STD17NF25 MOSFETs, but can be populated with any IGBT or Power MOSFET in DPAK or powerFLAT 6x5 package.
The board has a single-shunt sensing topology, and both the field-oriented control (FOC) and sensored or sensorless 6‑step control can be implemented.
You can find more details in the "Resources" tab of previous link.
2020-06-08 06:46 PM
Thanks for the reply, the board looks good. Does the hardware support to drive two BLDC motors synchronously, like Segaway did?
2020-06-16 02:31 AM
One board can drive one motor.
You can use two board and write the firmware to synchronize the movement as per your application.