2015-12-01 10:37 AM
Hello,
I set up the following minimal circuit to get started with the l6384e high voltage half-bridge driver[1]:2015-12-04 03:16 AM
I thought I checked for Vcc requirements. I should have rechecked before posting here.
The solution is that the l6384e has undervoltage lockout and in table 7 of [1]:Parameter Typ.
-------------------------- ---- VCC UV turn-on threshold 12V VCC UV turn-off threshold 10V Sorry for that. [1]: http://www.st.com/web/en/resource/technical/document/datasheet/CD00169715.pdf2017-06-07 02:17 PM
Hi, i'm having the same kind of problem with the L6384E. I'm using 12V on the Vcc, do you think it should works?
The strange thing about my aplication is the Vce, the voltage on Collector e Emissor doesn't get steady. As shown on the image.