cancel
Showing results for 
Search instead for 
Did you mean: 

for phase cutting control we would like use either BTA16 (T0-220AB) or T1635 (D2PAK) on ouer PCB.the controlsignal is a 3,3 VDC pwm. ( see attachment ) A T1635H-6T is placed instead the T1635 in the boom list by a mistake .

bmose.1
Associate

now we have following situation.

  1. the circuit works fine at using the BTA16
  2. at using the T1635H-6T the hase cutting doesn't works ( full wave is engaged over the PWM range )

Questions:

a. what is the difference between T1635 and T1635H-6T ?

b.how can we solved this problem ?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0