2014-07-29 9:04 AM
Hi,
I have a PMSM which I'm planning to run sensor-less. In case I run into problems with the sensor-less the motor I'm using also has a resolver fitted. I have a Resolver Decoder from analog devices so I'm wondering if I can read this over the SPI bus and input it to the FOC algorithim? Or should i use the quadrature outputs from the resolver deocder IC and run these digital inputs into the STM32. If i had more time I'd play around with some sample and hold circuits and use the spare ADC to sample the SIN/COS signals coming from the resolver and decode them into position in the STM32. But that's a little bit off for now. Regards, David Powell2014-08-12 8:44 AM
Dear David,
straightforwardly, you can connect the quadrature outputs to STM32 and enable encoder as auxiliary sensor; this way, for instance by enabling the DAC functionality, it's possible to compare - runtime - angle measurements from sensorless and resolver.
SPI is possible but need some FW development, of course.Regards,
Dino