2020-09-17 8:55 PM
Hi,
Is STTH1602CT Diode having Electrostatic Discharge voltage capabilities? if yes then how much voltage? Because its not mention in datasheet.
Thanks
Nandish Jasani.
Solved! Go to Solution.
2020-09-18 9:16 AM
Hello @Community member ,
The STTH1602CT is a standard dual diode with common cathode.
The two diodes have forward and reverse maximum voltage, as specified in the datasheet.
If you need to use a component in your system for ESD protection, I can suggest to visit the ST dedicated page here.
All the best !
2020-09-18 9:16 AM
Hello @Community member ,
The STTH1602CT is a standard dual diode with common cathode.
The two diodes have forward and reverse maximum voltage, as specified in the datasheet.
If you need to use a component in your system for ESD protection, I can suggest to visit the ST dedicated page here.
All the best !