2023-01-25 1:25 AM
I am looking for an alternative voltage regulator with similar functionality to the TLV76050DBZT. It needs to have an input of max 30v and output of 5v. I have attached the data sheet, It has to have the same pinout because the pcb cannot be redesigned at this current moment. It has to also be surface mount product with similar packaging.
Thank you!
2023-01-25 12:47 PM
Welcome, @AFour.1, to the community!
Unfortunately, we cannot offer an alternative in this case.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter