cancel
Showing results for 
Search instead for 
Did you mean: 

Add PWM control for a buck converter

federico.massimi
Associate III

Hello everyone,

   I need to make a dimmable buck converter. In practice, my requirement is to flash (<100Hz) a resistive load with variable duty.

The control signal is PWM from a microcontroller and the system is battery powered.

I searched the net but I didn't find a well-defined solution. What I wanted to ask is:

1) There are dc dc converter chips that have the PWM input to make the output flash?

2) How can I modify an existing buck converter scheme to add the PWM input?

3) Some converters have enable input, can I use this for PWM, could I have problems in the long run?

4) I saw that almost all LED drivers have this input, can I modify a driver LED to drive a pure resisitive load?

thanks in advance, FM

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0