cancel
Showing results for 
Search instead for 
Did you mean: 

About the TS3330AMR

Ikegawa
Associate

The TS3330AMR has a voltage reference, but the internal configuration of the IC is unclear.
Is a reverse bypass diode, like the reverse voltage protection of a linear regulator, unnecessary?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @Ikegawa, to the community!

Well, the data sheet clearly states in the absolute maximum ratings (table 1):

VOUT (Maximum voltage on the output pin) -0.3V to VIN +0.3V

So if the input voltage drops to zero and the output voltage of 3V is still present at the output due to large capacitors, for example, the max rating is violated without the Schottky diode mentioned.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Ikegawa, to the community!

Well, the data sheet clearly states in the absolute maximum ratings (table 1):

VOUT (Maximum voltage on the output pin) -0.3V to VIN +0.3V

So if the input voltage drops to zero and the output voltage of 3V is still present at the output due to large capacitors, for example, the max rating is violated without the Schottky diode mentioned.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.