X-CUBE-EEPROM software package, fills in zeros into emulated EEPROM on every reset.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-07-30 4:54 PM
I am using STM32L476, and I downloaded X-CUBE-EEPROM software package, included it into my project and it works fine. But I am noticing that after every reset it writes dummy word of all 0. CRC + Vaddress +Data... all 32 bits are zeros.
That write is issued from EE_Init() Step 8. Here is code snippet.
/*********************************************************************/
/* Step 8: Perform dummy write '0' to get rid of potential */
/* instability of line value 0xFFFFFFFF consecutive to a */
/* reset during write here */
/* Only needed if recovery transfer did not occured */
/*********************************************************************/
if (recoverytransfer == 0U)
{
status = VerifyPagesFullWriteVariable(0U, 0U);
/* The dummy write can be skipped in case pages are full
because in this case potential instability can not happen */
if ((status != EE_OK) && (status != EE_PAGE_FULL))
{
return EE_WRITE_ERROR;
}
}
Function VerifyPagesFullWriteVariable(0U, 0U); writes dummy 0’s.
Why is this done every reset? It slowly fills up my EEPROM with 0. It happens even if page is still in Active mode and there is a plenty of space to store new data in. There was no need for transfer.
This is how my EEPROM memory looks. I have some data with data zero values in first two locations, and next two locations are all zeros. And it keeps adding all zeros after every reset.
- Labels:
-
EEPROM devices
-
STM32L4 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-07-30 11:54 PM
which flash pages are you using? try to use the last two flash pages of your MCU and check again. Maybe you are writing to a flash page that already used for another purpose (for example firmware code).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-07-31 8:07 AM
I didn't change code from X-CUBE-EEPROM software package, so EEPROM starts at 0x08080000. The rest of my application is just basic. Not much of flash is taken by the application code which starts at 0x08000000.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-04 3:07 AM
I have noticed exactly the same issue. On each bootup and entire line of 0's is written to the page and slowly fills up the eEEPROM triggering useless switches.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-25 1:22 AM
I have noticed the same issue, too. Fortunately this behavior stops when the end of a flash page is reached (no page transfer is issued in this case).
Nevertheless this wears out the internal flash needlessly, because then a single data write of my application triggers a whole page transfer and the filling up with 0's starts again.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-03-14 6:52 AM
Hello,
This write of zeros in the initialization sequence has been added in order to make the EEPROM emulation driver robust to asynchronous resets and power-downs.
During the validation of the EEPROM emulation software, we noticed that sometimes, if an external asynchronous event (reset or power-down) interrupted a Flash write operation, then this Flash line was no longer writable. Reading that Flash line gave various results including 0xFFFF FFFF FFFF FFFF which did not allow to differentiate a corrupted Flash line from an erased line by performing a simple read operation. The solution to this issue was to systematically write zeros to the first available Flash line after reset.
Note that from a theoretical standpoint, the RM0351 and RM0394 warns that “The contents of the Flash memory are not guaranteed if a device reset occurs during a Flash memory operation.�? If you can guarantee that no external event will interrupt a Flash write operation, then you can simply remove the Step 8 of EE_Init function. This the case for instance if only entering Standby mode (which controlled by the application software) generates a reset and no other external reset is possible in the application.
But , if in practice, you cannot guarantee that an external reset or power down will occur during a Flash write operation, it is better to keep Step 8 of EE_Init in order to make sure the content of the EEPROM remains always valid.
Best regards,
Stéphane