2025-05-27 9:12 PM
Using NUCLEO H723ZG
I made a simple SPI module for communication as master
(this is the only module i am using)
I used the MOOC training on using SPI as a guide for programming
On observing clock
I found it to be discontinuous during transmit cycle - this puts the receiving slave SPI into error
0x84 code
See Scope shots of clock
I was wondering if any one else has seen this before
Thanx in advance for any suggestions/replies
Jay
Solved! Go to Solution.
2025-06-01 8:44 PM
Hi TDK
The dma trick seems to have worked!
Thanx for your help
solved-will close this case now
Jay
2025-05-28 6:12 AM
There is no issue in general with the SPI clock having delays between bytes. Most slaves have no issue with this. What chip are you communicating with?
If you don't want delays, reduce clock speed or consider using DMA.
2025-05-28 5:52 PM
Hi TDK
Thanx for replying
I was wondering
1) What would cause the clock to place delays ( i am not programmatically asking for delays)
The spi seems to be able to transfer about 13-14 words w/o delay
Why a new delay after 15th word?
2) Why would using DMA get rid of delay?
Also, The slave is a custom stm32H723 chip board
Jay
2025-05-28 8:10 PM
If the CPU can't keep up with data the SPI needs, there will be a delay between bytes.
Using DMA offloads this responsibility so no delays.
2025-06-01 8:44 PM
Hi TDK
The dma trick seems to have worked!
Thanx for your help
solved-will close this case now
Jay