cancel
Showing results for 
Search instead for 
Did you mean: 

Printf in Atollic still doesn't work correctly

SZoha
Associate II

Hi,

I am using the Nucleo-H743ZI, when trying to printf a buffer I see lots of data missing. Even when just trying to printf a counter I see the same issue, I tried it in Atollic as well as ST_LINK and I get same issue.

I saw many issues in the past and was able to find a solution to print something here:

https://community.st.com/s/question/0D50X00009XkhURSAZ/stm32h7-swo-printf-not-working

But still this causing the issue above.

I am using the code below in order to enable the ITM.

void ITM_enable(void)

{

*(__IO uint32_t*)(0x5C001004) = 0x00700000;

 //UNLOCK FUNNEL

 *(__IO uint32_t*)(0x5C004FB0) = 0xC5ACCE55;

 *(__IO uint32_t*)(0x5C003FB0) = 0xC5ACCE55;

 //SWO current output divisor register

 //This divisor value (0x000000C7) corresponds to 400Mhz

 //To change it, you can use the following rule

 // value = (CPU Freq/sw speed )-1

  *(__IO uint32_t*)(0x5C003010) = (*(__IO uint32_t*)(0x5C003010) & 0xfffff000) | 0x000000C7;

 //SWO selected pin protocol register

  *(__IO uint32_t*)(0x5C0030F0) = 0x00000002;

 //Enable ITM input of SWO trace funnel

  *(__IO uint32_t*)(0x5C004000) = *(__IO uint32_t*)(0x5C004000) | 0x00000001;

 //RCC_AHB4ENR enable GPIOB clock

  *(__IO uint32_t*)(0x580244E0) = *(__IO uint32_t*)(0x580244E0) | 0x00000002;

 // Configure GPIOB pin 3 as AF

  *(__IO uint32_t*)(0x58020400) = (*(__IO uint32_t*)(0x58020400) & 0xffffff3f) | 0x00000080;

 // Configure GPIOB pin 3 Speed

  *(__IO uint32_t*)(0x58020408) = *(__IO uint32_t*)(0x58020408) | 0x00000080;

 // Force AF0 for GPIOB pin 3

  *(__IO uint32_t*)(0x58020420) = *(__IO uint32_t*)(0x58020420) & 0xFFFF0FFF;

}

Thanks

Sharon

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

The issue in the other thread was *nothing* coming out. Are you at least getting some of the expected data?

What firmware version are you using on the ST-LINK ?

The above code presumes a 400 MHz CPU clock, and a 2 MHz SWD clock

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
SZoha
Associate II

Hi,

I am using ST_Link-V4.4.0.0

I do get the expected data but I can see that data is missing, as mentioned I did a test running a counter and printing the counter and I can see group of numbers missing. As the example below shows the left number is the counter (the right are numbers from the ADC-DMA) after sample 3091 the data is corrupted and you can clearly see some shift in the numbers that next correct sample is 4060. As I mentioned I can see it on ST-Link as well as Atollic.

I am using 400Mhz with  2 MHz SWD clock.

3087, 14658

3088, 23800

3089, 52624

3090, 64345

3091, 5

059, 45055

4060, 1684

4061, 62496

4062, 24112

4063, 13970

4064, 43582

4065, 11263

4066

Thanks

Sharon