2025-10-16 4:51 AM - last edited on 2025-12-29 9:43 AM by ELABI.1
Dear Sir ,
Kindly Help In Writing Program for PFC Boost Control.
As i have worked on making an power supply with Below Specification Details :
Input Voltage : 1 to 20 VAC(Variable)
Input Current : 3Amps (Constant)
We Require :
Output Voltage : 30VDC
Output Current : 3AMPS
For This we already created a closed loop system of power factor correction with boost controller .
in this we take feedback from output using voltage divider .
so i have an request to you kindly any one have solution pls suggest me to do this .
regards,
Nilmani
2025-10-31 4:49 AM
You should learn some basic electronics first.
The www is full of tutorials.
Please be careful with your hardware, don't get the idea of using any higher voltages.