Others: STM32 MCUs related

Find out more about STM32 implementations with external components, discuss use cases, and discover how to use new tools and ST components.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hello, I am currently working on STM32f205 using Keil uvision. I am getting an undefined instruction fault.

The core registers are as follows :R0 = 0 R1 = 0 R2 = 40005400 R3 = 70000 R12 = 802d8f9 LR = 800a88b PC = 8001ba0 PSR = 100002f- FSR/FAR: CFSR = 10000 HFSR = 40000000 DFSR = 0 AFSR = 0By disassembling the code, I found that the faulty instruction as ...

TBhil.1 by Associate II
  • 942 Views
  • 1 replies
  • 0 kudos

STM32 F3 I2C SCL Push-Pull Issue

We're currently using STM32F373CC micros in several of our designs. Part of our standard design has an EEPROM connected via I2C. We have our own hardware layer that is tried and proven over the decades. However, it relies on the I2C port pins having ...

GeoffF by Associate II
  • 4951 Views
  • 11 replies
  • 0 kudos

Error message tells me No source available for "__do_global_dtors_aux() at 0x80001ac". I can't seem to solve this problem, does anyone have any ideas?

Hello, I want to write/read on the flash memory. For that I made a small program (attached). My program works on Keil5 but when I switch to Atollic TrueStudio when I want to debug an error message tells me No source available for "__do_global_dtors_a...

EVesi.1 by Associate
  • 2427 Views
  • 4 replies
  • 0 kudos

TrueStudio_v9.3 for linux - https://www.st.com/en/development-tools/truestudio.html seems to be broken. I have been downloading it four times on two computers with Debian and Ubuntu and after unzipping received such message:

sudo ./TrueSTUDIO[sudo] password for eureka: ./TrueSTUDIO: 1: �zb�Yy׷G�j�ZQ�n��: not found./TrueSTUDIO: 3: Syntax error: Unterminated quoted stringmd5sum ./TrueSTUDIOd278f70667a1a216f2fc7f2ee4657996 ./TrueSTUDIO

MGoclo by Associate
  • 805 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L08xx EEPROM write fail

Dear,on STM32L083 I use internal eeprom. I found out, that when I use functionHAL_FLASHEx_DATAEEPROM_Programand during execution of this function the power voltage of mcu falls down (uplugged battery from device) - then in eeprom are saved wrong data...

JJRR by Senior
  • 1927 Views
  • 6 replies
  • 0 kudos

Resolved! how about the MCU using flash

I'm wanting to save user data (less than 50bytes) and factory data (less than 100bytes) to internal flash, however the user data may changes everyday and it may overrun datasheet's 10 K erases and writes. So whether the MCU or the other flash sectors...

0693W00000LzJQYQA3.png

Failure at line 13 in Target software startup scripts

Hello,I use STM32F407 MCU and when debugging with Attolic True studio v 9.3.0 I SOMETIMES got following error:Failure at line 13 in Target software startup scriptsError finishing flash operation. I attach linker and startup files.Any help will be app...

LPola.1 by Associate II
  • 1217 Views
  • 1 replies
  • 0 kudos

hello, I am using stm while controlling a device and after working conditions for a while, I saw that the software made itself like this. I have not encountered it on other devices. When I put the software on the processor again,it gets fixed,what reason?

That is part of broken softwareD8 0A 00 20 CD 02 00 08 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ...

0693W00000Lz1QVQAZ.png