2007-07-02 5:50 AM
2011-05-17 12:30 AM
Hi,
I am looking for a 3rd party providing Embedded Linux for the STR912. Thank you for your suggestions.2011-05-17 12:30 AM
Hi,
I think STR912 can not run Linux because there is no MMU on it, uClinux would work well. Jianhua2011-05-17 12:30 AM
Any news on uCLinux for STR912?
Thank you. RCR2011-05-17 12:30 AM
Hi,
actually, since the ST912 is based on ARM9, it _does_ have MMU. So, if uclinux supports this micro, it does without supporting the MMU (i.e. no memory protection). Does exist any free Linux support for this micro ? (from ST or for a third-party)2011-05-17 12:30 AM
Hi
There is now a pre-release version of the uTasker (OS,TCP/IP stack, device drivers and STR91XF simulator) available. Any one interested in beta testing (it has an IAR and Raisonance RIDE builds at the moment) is welcome. There is usually a board on-line at , so take a look - it is running on the Raisonance REva STR912F. Get full details at . Regards Mark Butcher