2024-10-17 02:50 AM - last edited on 2024-10-17 02:54 AM by Andrew Neil
i want modbus TCP/IP communication in my stm32f429 Nucleo board, for that i brought one W5100 module and connected module via SPI 1 port of controller, i also added io- driver library in my project tree from WIZnet for communication with W5100 module , when i am trying to ping from my lap cmd is showing destination host unreachable, i added W5100.h, socket.h, wiznet config.h file and respective c files also added to my project tree , any sample code available to check whether W5100 is communicating with my system.
Solved! Go to Solution.
2024-11-04 02:30 AM
Hello @rvishnu19 ,
I would recommend you follow the tutorial in Adding ethernet connectivity to a STM32-Nucleo
you can also check this Github Repo Serasidis/Ethernet_STM: WIZnet W5500, W5200, W5100 ethernet library for 8-bit, 32-bit Arduino and STM32F1 (STM32F103) micro-controllers and this stm32-nucleof4/stm32-nucleof4-ethshield1 at master · cnoviello/stm32-nucleof4.
worth mentioning that you need "TO ADD A RESISTOR 4k7 BETWEEN RESET AND 3.3V (OR RESET AND 5V) PINS ON ETHERNET SHIELD."
Regards
2024-11-04 02:30 AM
Hello @rvishnu19 ,
I would recommend you follow the tutorial in Adding ethernet connectivity to a STM32-Nucleo
you can also check this Github Repo Serasidis/Ethernet_STM: WIZnet W5500, W5200, W5100 ethernet library for 8-bit, 32-bit Arduino and STM32F1 (STM32F103) micro-controllers and this stm32-nucleof4/stm32-nucleof4-ethshield1 at master · cnoviello/stm32-nucleof4.
worth mentioning that you need "TO ADD A RESISTOR 4k7 BETWEEN RESET AND 3.3V (OR RESET AND 5V) PINS ON ETHERNET SHIELD."
Regards
2024-12-30 07:05 AM
Hello @rvishnu19 ,
any updates on this thread?
Regards