2025-01-12 10:24 AM
Hi at all.
Can VNLD5160 work with a normal STM32 CPU with 3.3V logical levels?
I don't find this information in datasheet...
Thanks...
2025-01-12 11:10 AM
Well, the data sheet mentions two important points:
Vsupply = VIN = 4.5-5.5V
This means that you either use a level translator or configure the GPIO of the STM32 as an open drain with external pull-up. As the VNLD5160 can only switch at a few kHz, the simpler and cheaper open drain variant may be sufficient.
Does it answer your question?
Regards
/Peter