2025-02-10 08:35 PM - last edited on 2025-02-11 12:49 AM by Peter BENSCH
I'm using the vnf1048f chipset.
k value is required for current sensing, but it is not specified in the data sheet.
Can you tell me what the k value is?
2025-02-11 12:49 AM
Welcome @gj, to the community!
The VNF1048F is not a high-side switch, but a high-side switch controller, where there is no K factor in the sense. Instead, measurements are taken via a shunt and the voltage dropping there is measured with a 10-bit ADC in a voltage range of 0...160mV (data sheet, section 3 and table 13 or table 45).
Does it answer your question?
Regards
/Peter