cancel
Showing results for 
Search instead for 
Did you mean: 

VND5160AJTR-E current sensing limit and output current limit

TStar.2
Associate

The datasheet does not explicitly call out maximum current that can be monitored with the "current_sense" pins but it appears to be 1.5A. Does that imply that this is also maximum continuous per output current that the part is rated to? Or is it 3.8A - the minimum short circuit current? Thank you.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0