2007-11-21 4:57 AM
2011-05-17 12:41 AM
Hi
Can you provide me with more details. Did vectors.s works with only one interrupt? regards MBS, [ This message was edited by: MBS on 10-04-2007 11:26 ]2011-05-17 12:41 AM
Hi
I looking for working vector.s file for Anglia Compiler I've got the standard vectors.s, but it doesn't work with two interrupts (from VIC0 and VIC1) [ This message was edited by: GrzesiekFl on 10-04-2007 10:33 ]2011-05-17 12:41 AM
I have two interrupts : one from TIM0 and one from UART0. When I use two interrupts I lose chars from UART0, but when I use ONLY TIM0 interrupts it works correctly
2011-05-17 12:41 AM
Hi ,
Please find attached a project (RIDE/IAR/RVDK) with two interrupts and note that RIDE is using GNU compiler (GCC-ARM) so, you'll find the necessary modification needed to vector.s in 91x_init.s . Regards, MBS [ This message was edited by: MBS on 13-04-2007 15:51 ]2011-05-17 12:41 AM
Hi,
Maybe your problem will be the cause of nested interrupt. also, I had same problem. would you modify the IRQ handler as following in the vect.s IRQHandler SUB lr,lr,#4 ;// Update the link register SaveContext r0,r12 ;// Save the workspace plus the current ;// return address lr_irq and spsr_irq LDR r0, = VectorAddress LDR r0, [r0] ;// Read the routine address ;//LDR r1, = VectorAddressDaisy ;//LDR r1, [r1] ;// Padding between the acknowledge and re-enable of interrupts ;// For more details, please refer to the following URL ;// ;//NOP ;//NOP ;//MSR cpsr_c,#0x1F | I_Bit ;// Switch to SYS mode and disable IRQ modified by KMSHIM, 2007/03/15 ;//MSR cpsr_c,#0x1F ;// Switch to SYS mode and enable IRQ STMFD sp!,{lr} ;// Save the link register. LDR lr, = IRQ_ReturnAddress ;// Read the return address. BX r0 ;// Branch to the IRQ handler. IRQ_ReturnAddress LDMFD sp!,{lr} ;// Restore the link register. ;//MSR cpsr_c,#0xD2 | I_Bit ;// Switch to IRQ mode and disable IRQ LDR r0, = VectorAddress ;// Write to the VectorAddress to clear the STR r0,[r0] ;// respective interrupt in the internal interrupt LDR r1, = VectorAddressDaisy ;// Write to the VectorAddressDaisy to clear the STR r1,[r1] ;// respective interrupt in the internal interrupt RestoreContext r0,r12 ;// Restore the context and return to the... ;// ...program execution. good luck!! best regards, KMSHIM2011-05-17 12:41 AM
Hi KM SHIM,
i think the problem of spurious interrupt are now solved with the different modifications that we have done on Vector.s and it.c . have a look to IRQ project which i send previously.(waiting for your feedback 8-) ) Regards, MBS :-] [ This message was edited by: MBS on 12-04-2007 11:52 ]2011-05-17 12:41 AM
Hi, MBS
Mode switch that you have done have been implemented in the IRQ handler. I think that there are jsut differences as like nested interrut and writing to VICx->VAR. Are there any difference in the your code? best regards, KM SHIM2011-05-17 12:41 AM
hi,
I didn't understand your question :( . The example which i sent,is a solution to generate correct nested interrupt with VIC0 and VIC1 without any conflict . did you try it? Regards, MBS [ This message was edited by: MBS on 12-04-2007 16:24 ]2011-05-17 12:41 AM
hi all,
i've done the portage of IRQ project to anglia IDE. :-] keep me informed about any issue. regards. MBS 8-) [ This message was edited by: MBS on 13-04-2007 17:38 ]