2021-12-01 6:49 AM
2021-12-01 9:40 AM
OK, in this case you can leave NC connected to GND, there is no internal connection.
But keep in mind that the M24C04 has a smaller EEPROM area than the AT24C32E.
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2021-12-01 7:10 AM
Maybe that was a typo and you meant the AT24C04C?
If this is the case, then AT24C04C and M24C04 have the same pinout, i.e. both have NC on pin 1.
Regards
/Peter
2021-12-01 8:53 AM
AT24C32E-SSHM-T have pin 1 ,2 and 3 to address. In this case all pins to ground.
2021-12-01 9:40 AM
OK, in this case you can leave NC connected to GND, there is no internal connection.
But keep in mind that the M24C04 has a smaller EEPROM area than the AT24C32E.
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter