2025-01-21 1:39 PM - last edited on 2025-01-21 3:23 PM by Peter BENSCH
We are working on one of our project which previously using TDA7566 IC.
Can anyone suggest any pin-to-pin compatible IC for TDA7566?
Are the following IC's are compatible - TDA7580, TDA7388, TDA7850?
I would like to know more about the 3 pins (pin number: 22, 25, 4) of TDA7566 as there are mainly 3 pins which are not match with TDA7384A & TDA7385 and similar case with other IC's.
2025-01-21 3:47 PM
Welcome @Raj23, to the community!
As you may have seen, the TDA7566 has been discontinued for a long time. Pins 22, 25 and 4 in question provided functions that are unfortunately no longer included in any other class AB amp still available: I2C Clock/Data and CD_Out (Clip Detector Output). These pins are used by all the alternatives as MUTE, DIAGNOSTICS and ST-BY.
I'm sorry, but apart from remaining stocks of the TDA7566, which you may find somewhere on the Internet, I can't give you a pin2pin compatible alternative if your project uses the pins mentioned.
Regards
/Peter