2003-12-03 5:53 PM
STVP7 / ST7FLITE29 and option bytes
2003-12-01 6:18 AM
Hi,
coming from ST62, I am new on ST72-series and need your help. I shall program a ST7FLITE29 installed in design-kit ST7MDT10-EPB using STVP7 ST7 visual programmer. My goal: At 5Vdd run the internal RC oscillator (=1MHz) to produce 8MHz and enable LVD at optimum level. Please point out the correct option byte selections for: ''OSC RANGE'' ''PLLx4x8'' ''PLL OFF'' ''PLL32 OFF'' ''OSC'' ''LVD'' I would be grateful for any tip. Regards, Tomas2003-12-03 3:11 AM
The option byte settings for your requirement are-
''OSC RANGE'' - Select default value(i.e external clk source-CLKIN on PB4) ''PLLx4x8'' - PLLx8 ''PLL OFF'' - PLL enabled ''PLL32 OFF'' - PLL32 Disabled ''OSC'' - '' RC oscillator ON'' ''LVD'' - Select LVD level as per your requirement2003-12-03 5:53 PM
Many thanks !
Best regards, Tomas Fahlman