2004-10-11 11:02 PM
STVD with Cosmic and Metrowerks,step by step instruction ?
2004-09-30 12:24 AM
any brief step by step instrcution to create new workspace,then toolchains path and prohject settings so that build can be succeed?
try using the Cosmic workspace sample in ST7 Software Library 2.0, the build is failed!2004-09-30 12:51 AM
Try using Rebuid all option for first time.
For which device you want to create workspace, ST7Library has ready to use workspace for different devices. Also configuration files (.mak,.prm and .lkf ) for most of ST7 devices are available at device\cosmic or devices\metrowerks path. Hope this helps Thanks and Regards, PraveenG2004-10-05 9:54 PM
Hi Kuni,
you can find more information on how to create a Cosmic, Hiware or Assembler project for STVD7, reading the SofTec Application note AN002, this is the link: Cheers, Nicola2004-10-11 11:02 PM
using workspace of ST7LIB2 or ST7FMC download from web site,
in project setting Maker : Gmake Maker filename : C:\COSMIC\EVALST7\gmake but there is no gmake file in my C:\COSMIC\EVALST7 what should I modified in the project setting in order to make the Build succeeded ?