2007-06-15 05:01 AM
2007-06-11 01:56 AM
Hi chaps,
The STR755 doesn't have a USB peripheral. In the LQFP100 package, there are USB pins. Does anyone know their function when there's no USB peripheral in the device? I presume this carries through to the STR752 too. Cheers, Peter2007-06-13 02:36 AM
Hello,
For the 64 pin package, pins 41 and 42 are shared with USB and CAN. depending on device part number. For example, the STR752FRx only CAN is available. The 41& 42 pins are mapped to P0.15/CAN_TX and P0.14/CAN_RX. In addition, the non available pins on LQPFP64 and LFBGA64 packages are internally tied to low level. Regards.2007-06-13 09:47 PM
Thanks coucou. Do you have any information on the LQFP100 package?
Regards2007-06-15 12:00 AM
Dear peterwrigley,
For the LQFP100 package, when there's no USB peripheral in the device as STR755FVx part number, the corresponding USB pins should be left unconnected and not used. Thanks.2007-06-15 05:01 AM
Thanks coucou, that's exactly what I was after!